Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

I am a thesis student and I have to build a bare-metal application to make the two CAN subsystems on SPC58NN84x MCU communicate, starting from bare-metal application for CAN testing on implemented by default on SPC5 studio, how can I do this?

I have used the default test bare-metal application for the testing the can in SPC5 studio stopped the loopback, swap the RX ID filters in the configurator, and tried to send using one can subsystem and receive by the  other but it keeps stuck in th...

ZMoha.1 by Associate II
  • 10366 Views
  • 5 replies
  • 0 kudos

Resolved! I2C communication with non-existing slave

Hi. I'm trying to send a message to a non-existing slave via I2C on SPC58EE84E7.Is this possible?I get a NACK error message in response. Are there any examples of such an implementation?Thank you!

David_D by Associate II
  • 1400 Views
  • 1 replies
  • 0 kudos

SP5C studio v6 not launching

Hello! I'm new to SPC5 studio. I just downloaded and installed the software. when I try to launch it, nothing happens. my laptop: Lenovo Ideapad 320, i5 7th gen, 8gb ram, Windows10what I tried:-I tried launching in compatibility mode(windows 7,vista)...

NSent.1 by Associate
  • 898 Views
  • 0 replies
  • 0 kudos

Resolved! Serial DMA position

Hi,I am developing an application on SPC58EC that uses the serial with DMA for reading.I'd like to know if there is a way to know and get the position where it's writing in the buffer. I mean something like the corresponding "__HAL_DMA_GET_COUNTER(.....

RD'Ig by Associate II
  • 2060 Views
  • 2 replies
  • 0 kudos

Resolved! SARADC with DMA in SPC58EE84E7

HelloI intend to use SARADC with DMA and I'm not able to configure it. SPC5 Studio provides examples that I'm using but in the configuration options of other SPC5 models in SARADC Configurations the option DMA configuration appears. On SPC58EE84E7 do...

EReis.1 by Associate
  • 1461 Views
  • 1 replies
  • 0 kudos