Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Hi, I'm evaluating a solution for a 1 ms reading using the SDADC driver provided with the SPC Studio (SPC58NE). I found this check in the code, that sometimes causes a missing reading. I add a comment with the SFR register that I'm currently using.

uint8_t sdadc_lld_read(SDADCDriver *sdadcp, float* converted_value) {   int16_t data; uint8_t return_value = SDADC_DATA_NOTVALID;   /* check if valid data is available */ if (sdadcp->sdadc->SFR.B.DFEF == 0U) /* <- Check if the FIFO is not emp...

VBOSC.1 by Associate
  • 2083 Views
  • 2 replies
  • 0 kudos

Resolved! UDE starterkit debugging problem

I am using SPC58EC disp board. I can upload code and see led is linking when I reset the board. But I can not debug it, my code’s start location is 0x01020000 but it is going somewhere else. I asked if I can set debug start location to PLS and they s...

kb24 by Senior
  • 1963 Views
  • 2 replies
  • 0 kudos

Resolved! Alternate for ST10R

Hi Team,We are using ST10R167 in our design, as you that it is obsolete right now. So we have chosen an Alternate MCU, Part Number:SPC560P50L5CEFAR.Please let me know the Year to End of Life of the selected MCU and your comments on this Alternate.Loo...

GPand.3 by Associate II
  • 1952 Views
  • 1 replies
  • 0 kudos

How can i use flexray on SPC584B-DISP development board?

Hello , i bought one SPC584B-DISP discovery board. And i think there is a Flexray Peripheral mcu on the board because mentioned that on ST's website: SPC584B-DISP - SPC584B-DISP: Discovery kit featuring SPC58 4B Line MCU in eTQFP144 - STMicroelectron...

AYazı.3 by Associate II
  • 1529 Views
  • 1 replies
  • 0 kudos
coolboy by Associate
  • 1838 Views
  • 2 replies
  • 0 kudos

Resolved! SPC5/UDESTK debugger loading incorrect value in core register

Hi Team ,We are using PLS debugger for one of our project ST SPC58NG84E7 controller ,compiler GHS Version 202114 and Debugger UDE STK2021 .But we are facing one issue while debugging one function in SetAbsAlarm(1,10,10) In SetAbsAlram while we debugg...

PKUMA.3 by Associate
  • 1208 Views
  • 1 replies
  • 0 kudos

Resolved! I'am wondring if there is any application note or document about CAN bootloader for SPC584B? this bootloader does it support UDS protocole? What is the tools used to validate CAN bootloader on this product?

I'am working on automotive project that the client need a validation plan for automotive device using SPC584B MCUI have did a search on st.com site to find somthing about CAN/UDS bootloader but i did'nt find the appropriate document for my need.any s...

ZBen .11 by Associate
  • 1359 Views
  • 1 replies
  • 0 kudos