Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5Studio license expired after 1 year trial

Hi, my license for SPC5Studio is expired after 1 year trial. Is there any way to extend this license? I do have a permanent license but it's activated on another Lab PC (connecting to a UDESTK dongle). I need to activate it on my personal PC so that ...

TBui.1 by Associate
  • 3910 Views
  • 1 replies
  • 0 kudos

Chorus 10M Performance Monitor APU Event Mapping

Hi,I want to utilize the Chorus 10M Performance Monitor APU. In the reference-manual rm0004-programmers-reference-manual-for-book-e-processors-stmicroelectronics.pdf Section 3.16.3 Table 55 which shows the Mapping of the PMLCax Register bits you can ...

WMuel.1 by Associate
  • 1084 Views
  • 0 replies
  • 0 kudos

Having Difficulties Figuring Out How to Flash the MCU

I'm using the AEK-MCU-C4MLIT1 evaluation kit for testing out the SPC58 MCU's. I have managed to write, generate, and build my program but I can't figure out how to actually upload my code onto the SPC58. I am coming from the STM32 MCU family where ...

ZGood.1 by Associate
  • 1439 Views
  • 1 replies
  • 0 kudos

SPC560P44L3 Center alignment PWM generation.

Controller: SPC560P44L3 (Custom board)IDE: SPC StudioIm facing problems in generating 16kHZ frequency PWM center alignment.For frequencies below 500Hz I was able to generate PWM center alignment, as per the code generation settings. But going for hig...

RRama.3 by Associate
  • 1495 Views
  • 0 replies
  • 0 kudos

Reset line driven low on SPC58E

Hello guys,We have designed a board based on SPC58EG40 MCU, this MCU is designed to be programmed via spc5-udestk, all the connections are fine except the Reset line which gives a value of 0.5V, even though it's pulled up to 3.3V by a 4.7Kohm Resisto...

Basel by Associate II
  • 1299 Views
  • 0 replies
  • 0 kudos

SPC58EC-DISP Serial Communication Sample code HELP!!!

A problem occurred during the serial communication test process with the SPC58EC-DISP board.The test environment and problem symptoms are as follows.​test environment1. Apply 12V Power to SPC58EC-DISP board2. Debugging and Serial Communication Test t...

SMOON.21 by Associate
  • 9403 Views
  • 9 replies
  • 0 kudos