Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Why SPC560P40 trigger swt reset?

I've been feeding dog, but sometimes it still triggered swt reset.I can get reset info from reading DES and FES register.WHY??Who can tell me the FAE or technical department e-mail in China?Or tell me the reasion?

SPC582B - writing boot-loader to be used with BAF

I would like to write a simple boot loader to be uploaded to SPC58's RAM by BAF (according to "Boot Assist Flash" section of RM).The boot loader's job is to receive the program by LinFlex or CAN and store to MCU's flash. All this without need of usin...

Yannek by Associate III
  • 4971 Views
  • 5 replies
  • 0 kudos

SPC58xG : FCCU error CPU 0 lockstep disable

HiI try to apply the safety guide on the SPC58xGThe FCCU is a main part to check the error on the SPCx58, but I have several problems.1) FCCU Status error.The status register has this value (after clearing, and read flowing in x0A mode)FCCU_RF_S0 = 0...

MRO by Associate II
  • 1008 Views
  • 0 replies
  • 0 kudos

How to select the ADC mode from scan (default ) to one shot mode? Should I want to edit the Low Level Driver to change the mode which is in MCR register?

I am usingSPC56Ecxx. I need to change the ADC mode from scan (default) to one shot mode. There is no options provided in SPC5 studio. ADC MCR register has the option for mode selection.Should I want to change in LLD or any other option to change the ...

SPC584Bx chip. Some error occurred while downloading to the UDE SDK tool. How to clean or erase all in the flash for initilize?

We are developing products with SPC584Bx chip. The following error occurred while downloading to the UDE SDK tool:Tu 14.03.2023 17:51:12.822, Success, Core2, UDEDebugServer, Connection to SPC584B70 target established: PowerPC Target, JTAG-ID: 0x20144...

0693W00000aJ5HJQA0.png