Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! AUTOSAR MCAL Drivers is free or licensed?

Hi fellas,Whether STM's SPC5x AUTOSAR MCAL is free or licensed version. Also, its been told, it provides CDD and no AUTOSAR OS,for which FreeRTOS is used. Whether this FreeRTOS version for AUTOSAR is free/licensed?

Resolved! SPC574S64 Crystal Confuguration

Hi I am working on SPC574S64 Controller, A20MHz Crystal is used in our boardI tried to configure it in the SPC5StudioI tried using one of the example code for the configuration where a 40MHz is used in the configuration and I tried to change to 20MHz...

_legacyfs_online_stmicro_images_0693W00000bi2xqQAA.png
VP.6 by Associate II
  • 3411 Views
  • 4 replies
  • 0 kudos

SPC574S Issue with UDESTK debugger

Hi All,​I am working on SPC574S64 Controller​I am using the sample code from the SPC5 StudioPIT Time which toggles the port for 4ms, 2ms and 1ms​I have also observed one more issue with the crystal, I couldn't see the oscillation but could be my logi...

_legacyfs_online_stmicro_images_0693W00000biB6VQAU.png _legacyfs_online_stmicro_images_0693W00000biB6aQAE.png
VP.6 by Associate II
  • 1182 Views
  • 0 replies
  • 0 kudos

Hello everyone, I am using a SPC584B70E5 microcontroller and I am trying to tell it a new application entry code after it wakes up from Standby Mode. Are there any methods to do it ?

I have two firmware saved into my Flash Memory at two different addresses (the former is a bootloader and the latter is my main application). After the micro is entered in Stanby Mode, I wish it would just load only my main application, skipping the ...

FCola.1 by Associate III
  • 1120 Views
  • 0 replies
  • 0 kudos