Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC58 : CAN communication

While CAN communication run.If error occurs...(ex. bus_off, error passive, warning status ./... )How to reset?

hans536 by Associate III
  • 2520 Views
  • 1 replies
  • 1 kudos

Resolved! Can EVALSTDRIVE101 drive a BLAC motor?

hello everyone, i'd like to know if i can use the EVALSTDRIVE101 add-on board driven by an stm32-nucleo to drive BLAC motors. Because the datasheet says that they are suitable for BLDC AND PMSM.Otherwise there is some other board that allows driving ...

Resolved! Task on GTM DPLL loss lock callback in ECU?

Anyone here do ECU project with GTM on SPC57?what task/function should I add on loss lock callback of the GTM DPLL? I saw some samples project, they switch to half cycle ( 360 degree ) on the loss lock callback event. but I still have no clue the ben...

jmary by Associate III
  • 2677 Views
  • 2 replies
  • 0 kudos

Resolved! How to start up with Stellar SR6 P7

I have shortlisted the following microcontroller https://www.st.com/en/automotive-microcontrollers/sr6p7c8.html#tools-software for one of the protoype demonstration. For this prototype development, I will be using MATLAB Simulink, to create a model a...

AkshC by Associate II
  • 3953 Views
  • 4 replies
  • 0 kudos

Resolved! SPC 5 for MacOS

I loved the approach that STM32 had a IDE for MacOS. It looks like there is none for SPC5. Is that correct? I would love to start developing with SPC5 and my newly bought evaluation board, but the download page only features a .exe file.. 

Orbiter by Senior
  • 2091 Views
  • 2 replies
  • 0 kudos