cancel
Showing results for 
Search instead for 
Did you mean: 

Can EVALSTDRIVE101 drive a BLAC motor?

Nicholas_minafra97
Associate

hello everyone, i'd like to know if i can use the EVALSTDRIVE101 add-on board driven by an stm32-nucleo to drive BLAC motors. Because the datasheet says that they are suitable for BLDC AND PMSM.

Otherwise there is some other board that allows driving  blac motors?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

STEVAL-IPM15B Can work with STM32 boards but it supports DC Motors not AC.

Best regards.

II

View solution in original post

3 REPLIES 3
Issamos
Lead III

Hello @Nicholas_minafra97 

As you can see in this description 

Screenshot_2023-09-05-16-31-41-51_40deb401b9ffe8e1df2f1cc5ba480b12.jpg

The EVALSTDRIVE101 is designed to drive three-phase brushless DC motors.

That's why it can't drive BLAC motors.

For AC motors driver, I suggest you to take a look at this .

Best regards.

II

Nicholas_minafra97
Associate

hello, @Issamos 

Can you tell me if STEVAL-IPM15B can be driven by a stm32-nucleo and if it can drive a BLAC motor ?

thank you.

 

STEVAL-IPM15B Can work with STM32 boards but it supports DC Motors not AC.

Best regards.

II