Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC572 with SARADC in DMA mode

We have the SARADC up and running in DMA mode on 1 channel as per the sample application.But when we add 2 more channels we can't get it to go throgh the callback routin. (saradcconfdma_ch1_conf_cb & saradcconfdma_ch2_conf_cb) and hence we don´t get ...

Larsa by Associate III
  • 1689 Views
  • 0 replies
  • 0 kudos

SARADC errors after SPC5 uppgrade

Worked perfect 2 years ago, then after updating the SPC5Studio we can´t get the SARADC to compile without alot of errors in the saradc_lld_cfg.c file (attached picture). We tried to use the old saradc_lld_cfg.c file and we could compile it but the ad...

Larsa by Associate III
  • 2773 Views
  • 1 replies
  • 0 kudos

Error encountered while building the code

./components/spc574sxx_low_level_drivers_component_rla/lib/include/spi_lld.h:690:2: error: #error "SPI driver activated but no DSPI peripheral assigned"#error "SPI driver activated but no DSPI peripheral assigned" This is the error i encountered whil...

SPC5 GTM Cluster Clock issues

Using the SPC572Lxx RLA GTM DPLL Test Application for Discovery all works fine until for some reason the Cluster Clocks in the Clock Manager Unit of the GTM IP Configuration changes to what´s shown in the picture and we get the Error "2' is not a val...

Larsa by Associate III
  • 1660 Views
  • 0 replies
  • 0 kudos

FDA903D unable to play audio out on custom hardware

Hello All, We have designed our own custom hardware using SPC582bxx automotive controller and FDA903D audio amplifier. We built the code test the audio amplifier, code is very simple to play audio. We have used SPC582Bxx Engine simulator code and mod...

Resolved! SPC58EC80 CanBus RTR Frame Request

I'm using SPC58 DISP Board for RTR request data frame from a battery pack. I have set the RTR value as 1, but didn't receive any reponse data frame from the battery. I have tested with CAN analyser, reponse data frame is coming(working fine). When I ...

Screenshot 2024-06-19 185331.png

Resolved! Reference Design

I am MURAL SELVAM from India. I am Currently working on Automotive project I need reference Design for Below given part number..SPC560D30L1B4E0XIf You have any reference design kindly provide me.

murali by Associate III
  • 1958 Views
  • 1 replies
  • 0 kudos

CAN1/2 DMAMUX on SPC58 2B

Hello,Looking through the reference manual for this chip on page 111 (RM0403 R7) it looks like there is a DMA peripheral line from CAN 1 and CAN 2 to the DMA module. I can't seem to find any reference to this on the MCAN side though or how to enable...

OHarc.1 by Associate II
  • 1786 Views
  • 2 replies
  • 0 kudos