Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Help me for reading and write SPC570s

Hi, MY name is Metropolis and search support for reading and write this mcu. Mcu is spc570s, i'm search information on web and not have find. Thanks for you support, i'm search Data sheet correct and tools for reading and write. King Regard

Resolved! Stellar Studio CAN Filters

Hi ! We are using an SR5E1E7 with StellarStudio. But we are struggling with CAN filters. How to setup the CAN device so it can accept any CAN-ID? Or better, how mask work for the CAN Filters ? We are using CanOpen and we can't really set every ID we ...

sacha_0-1743524208706.png
sacha by Associate II
  • 995 Views
  • 1 replies
  • 0 kudos

Unable to connect Debug_JTAG

Hi,I'm unable to connect to JTAG to debug the ECU after having successfully flashed via JTAG.Getting a message "Debug port fail" --> attached screenshot for more info.I would appreciate any insight into the potential causes of this failure. Thank you...

SPC560P34L1 Data Flash Write

Hello I want to program the data flash in the SPC560P34L1 microcontroller.  The user's manual says that double-word (64 bits) data page programming is supported, but an errata, DocID024694 Rev 4 (SPC560P34x, SPC560P40x devices errata JTAG_ID=0x2AE2_2...

SPI Clock Error and affect CAN module

Hi I am developing my project using the SPC58EC74 chip,I found two problems when using SPI(The clock I/O is PG[11]/DSPI0_SCK, which is pin 34)。first question:When the amount of my code is relatively small, the clock signal is normal; when the amount ...

企业微信截图_17419580905310.png 企业微信截图_17419587014929.png

Resolved! PLS Problem

Hi,i have used PLS many time and many.Now PLS does not work any more. Still this problem: Message from component 'PpcJtagTargIntf' :Can't connect target !Message from component 'PpcJtagTargIntf' :No JTAG client found !Please check:- target power supp...

Resolved! Get core ID with SR5E1Ex

Hi,I'm developing a bare-metal project with the SR5E1Ex (E3 and E7), and need to determine the current core ID at run-time.Could you please confirm if there are any registers that can be read to determine the current core ID? The only multicore examp...

Resolved! GetCoreID with SR5E1

I'm developing Autosar OS for multicore project for SR5E1 MCUOS needs to know which core is running.But I can't find any register which contain this infomation.Anyone know how can I GetCoreId with SR5E1 MCU?

phuongle by Associate
  • 5004 Views
  • 5 replies
  • 0 kudos