2024-12-10 12:08 AM
I'm developing Autosar OS for multicore project for SR5E1 MCU
OS needs to know which core is running.
But I can't find any register which contain this infomation.
Anyone know how can I GetCoreId with SR5E1 MCU?
Solved! Go to Solution.
2025-03-05 3:25 AM
Hello,
unfortunately using the SR5E1 is not possible to understand the core running directly reading an unique Id; as a workaround it is possible to do this via software for example reading the address of the Vector Table that will be different between cores. An example is done in the StellarESDK in the muti cores example.
Best regards
Francesco
2024-12-12 12:25 PM
Hi phuongle
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards
Joe
STMicro Support
2024-12-20 8:37 AM
Hello Joe ,
Sorry for the late answer ,
which version of StellarESDK do you use , 1.8.0 ?
Best Regards
Erwan
2025-02-21 4:38 AM
Hi. I'm also having the same issue of trying to determine which core is currently running. I'm not using any SDK, as this is being tested "bare metal". Any updates on how this can be accomplished?
Regards,
Steven Daglish
2025-03-05 3:25 AM
Hello,
unfortunately using the SR5E1 is not possible to understand the core running directly reading an unique Id; as a workaround it is possible to do this via software for example reading the address of the Vector Table that will be different between cores. An example is done in the StellarESDK in the muti cores example.
Best regards
Francesco
2025-03-06 12:36 AM
Thanks for your response! I had workaround solution by using software solution too.
No more concern from my side
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.