Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

unhandled exception

Posted on December 21, 2017 at 14:42i am developing boot loader for spc56ec64l7 controller.my bootloader application is at address 0x00 and boot loadable application is from 0x0001_0000. i integrate flash driver from one demo project.when i try to u...

karan by Associate III
  • 1759 Views
  • 1 replies
  • 0 kudos

SPC560B64L7 FlexCAN bootloader

Posted on December 18, 2017 at 04:05Hi, I'm currently using a SPC560B64L7 and I wish to go into bootloader via FlexCAN without connecting pin PA[8] and PA[9], is this possible to do so? Best if I could do all this in my application code.

Poon Jon by Associate
  • 1108 Views
  • 1 replies
  • 0 kudos

Resolved! Connection between SPC5 Connect and SPC560B64L7

Posted on December 13, 2017 at 10:59Hello, if i wanted to program the MCU using SPC5 Connect via CAN, what kind of connection did I need to make between SPC5 Connect and the MCU? The MCU I currently using is SPC560B64L7.

Wong JS by Associate II
  • 3011 Views
  • 5 replies
  • 0 kudos

Resolved! How to use SD2 for Serial read/write on SPC570S-DISP

Posted on December 12, 2017 at 02:55Hi,I am using sample application for serial operation on SPC570S-DISP, from serial_lld.c, it looks like SD1 is mapped to LINFLEX0 and SD2 is mapped to LINFLEX1. I have no problem read/write SD1, however i need at ...

Job Shen by Associate III
  • 3168 Views
  • 4 replies
  • 0 kudos

spc5.drive.cloudforge.com

Posted on December 13, 2017 at 16:45SPC5Studio 5.7.0 is available Dear All ,SPC5Studio 5.7.0 is available*** Highlights ***Here are the changes coming with SPC5Studio v5.7For Mass Market:   ===========- Windriver support (see application level) - mi...

Resolved! Looking for BSDL file for SPC564A70L7

Posted on December 11, 2017 at 11:10Hello,I am looking for the BSDL file for the SPC564a70L7. This is the LQFP176 package.Does anyone have the BSDL file?

Resolved! UART access on SPC570S-DISP board

Posted on November 30, 2017 at 02:49Hi,I need to use UART to send data from the SPC570S-DISP to a different board, looking at the UM2025 User Manual for the SPC570S-DISP: Discovery + Evaluation Board, section 2.9 LINFlex and UART, it says the LINFle...

Job Shen by Associate III
  • 4084 Views
  • 7 replies
  • 0 kudos