Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! How to config with CAN bus filter in SPCstudio?

Hi all, I'm using SPC570S0DISP DEMO Board(SPC570S50E1) to lean how to config CAN's filter.And the attachment is my config and source code. In my config,i just want CAN ID 0x112 to interrupt fifo callback function.And then i get the data in call...

LJere by Associate
  • 1858 Views
  • 2 replies
  • 0 kudos

Resolved! Confused between set address for bootloader and 32-bit store address from UART/CAN flash while flashing

Hi,This is for SPC560Bxx. I need clarification on set address for bootloader and the 32-bit address that shall be mentioned on UART/CAN frame. There is one column in firmware updater component, where we are supported to choose it the set address, he...

Resolved! GCC compile and flash code

Is it possible to compile the application only with Gcc (free) so do not use GHS or Hightec and flash and run the compiled code?I can tolerate that this compiler is not efficient as those not free.

gp73 by Associate III
  • 1050 Views
  • 1 replies
  • 1 kudos

Resolved! Choose MCU family

Goodmorning,    I've been using the STM32 MCUs for a while. Now I should start a safety critical project, nothing complicated, I just have to monitor a signal at precise time intervals and set some GPIO (an interrupt based on a timer and little else)...

Resolved! difference between SPC5-UDEDEBG and SPC5-UDESTK-PLUS?

For starting with development on SPC56ELxx what I need is:the discovery board : https://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-mpu-eval-tools/spc5-automotive-mcu-eval-tools/spc56l-discovery.htmlSPC5 Studio...

gp73 by Associate III
  • 1115 Views
  • 1 replies
  • 1 kudos

download.spc5studio.com

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/SPC58xHxx, Advanced GTM and USBTypeC credentials should be requested on credentials@spc5studio.comNew or updated componentsRLA 1.10....