Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Help in finding STV0991 SDK and example codes

Hi,We are interested in using the Smart Automotive Cameras reference for our WiFi Camera Project. But we were unable to find any SDK/example codes related to the solution, So could you guys please help us in finding the required software's.Regards,I...

DIDS by Associate
  • 904 Views
  • 0 replies
  • 0 kudos

SPC560P40 series Bootloader

I want to develop a bootloader for SPC560p40l3 controller.I've read about BAM and SBL.But that method is Hardware dependent, i.e we've to give 1 logic to a[4] to get it into boot mode(CAN/UART).I don't want to use the internal Boot module.Is there an...

Aakash by Associate
  • 1618 Views
  • 1 replies
  • 0 kudos

Where can I find the example project for JTAG over CAN?

I'm implementing JTAG over CAN as described in AN4345, "Debug over CAN". https://www.st.com/resource/en/application_note/dm00094335.pdfIn sections 5 and 6, mention is made of an example Greenhills project with the code described in the app note. Desp...

ehntoo by Associate
  • 996 Views
  • 0 replies
  • 0 kudos

Resolved! Not able to send the data without delay in UART interfacing. I am using 3 UART channel at a time. I want to know how can I remove the delay .

I am working with 560B54L5 discovery board. I am using runtime IO component with uart test application. I am able to send data at one channel at a time(one channel).my issues arehow to receive the data using interrupt in case of runtime IO?How can I ...

rpoon by Associate II
  • 1911 Views
  • 1 replies
  • 0 kudos

Resolved! Creation of a timer for continuous execution

I used the stm application fot configuaring the Timer.1.first picture shows the timer is working for just 4 seconds but i want it to run continously i used the stm_lld_enable inside the for loop and it is not working i dont know why.

RRama.8 by Associate II
  • 1926 Views
  • 2 replies
  • 0 kudos