Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Bootloader example code for SPC560P50L3 controller

Hi All,I'm searching for example Bootloader code for SPC560P50L3 controller ( 100 pins package). I tried import from the example code in SPC5 studio, but it is for a SPC560P50L5 controller. How I can convert this code SPC560P50L35controller ( 144...

How can I find and download the source code of the library referred by the RM0020 - Reference manual - SPC56xx and RPC56xx DSP function library 2. (DocID14728 Rev 3 - 2015)

I read the manual and I could not find the location of the library to download. Does anyone know where it is located or if there is? Is it available through a third party or from another website? Is there an equivalent one somewhere else?Any help wou...

CGube.1 by Associate
  • 1073 Views
  • 1 replies
  • 0 kudos

L9779WD-SPI example code!

Hi,L9779WD-SPI is an excellent IC for automotive, with the exception of it's datasheet.SPI communication section of datasheet confused me and other engineers of our section!We read 0xFFFF in the first write/access to registers, a data on then next w...

MAC_ADDRESSn_HIGH127_64 register @ SPC58 G Line MCUs ?!

Hi all,I was reading the TRM titled:SPC58xEx/SPC58xGx 32-bit Power Architecture® microcontroller for automotive ASILD applicationsHere is the TRM Link:https://www.st.com/resource/en/reference_manual/dm00148989.pdf I am focusing on the Ethernet module...

MNabi.1 by Associate
  • 666 Views
  • 0 replies
  • 0 kudos

download.spc5studio.com

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/SPC58xHxx, Advanced GTM and USBTypeC credentials should be requested on credentials@spc5studio.comNew or updated componentsRLA 1.11....

I am using DFLASH for storing data at multiple locations. Code is attached below. "READ MEMORY BLOCK FAILED" error.

#include "components.h"unsigned int i, location_no, data[9];int main(void){ /* Memory Unlock */ DFLASH.LML.R = 0xA1A11111;  //write password DFLASH.LML.R = 0x00000000;  //unlock all 4 16k blocks DFLASH.SLL.R = 0xC3C33333;  //write password DFLAS...