Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Issue in Flashing the SPC584B- DSM board

Hi Team,Please help to resolve the issueFlashing the SPC584B- DISP board failed and end up in the following errors,  Error messages:  PpcJtagTargIntf: Connection to target lost !  PpcJtagTargIntf: Failed to reset target system !  PpcJtagTargIntf: No...

VPAI.1 by Associate
  • 2088 Views
  • 2 replies
  • 0 kudos

ai.spc5studio.com

Dear All ,SPC5Studio 6.0 is availableyou can download it in this following link :https://www.st.com/en/development-tools/spc5-studio.htmlFoundation 6.0 (installable with product installer only)New OpenJDK 11 java runtime environment distributed with ...

L9637 - LIN Bus - ISO9141 - K-Line

Hi,I'm designing an automotive scan tool. For now, I'm studying about ISO 9141 and LIN Bus compatibility. I have a legacy hardware that uses L9637 to perform ISO 9141, but I want to add LIN capabilities in a new hardware.So, I would like to know if t...

DFlor.1 by Associate
  • 2906 Views
  • 2 replies
  • 0 kudos

How to use aek-com-blev1 demo code ,some files are missing?

I am interfacing AEK-COM-BLEV1 with SPC58ECXX .I imported the ble demo code from autodevkit but while compiling it is giving some errors like:In file included from main.c:19:0:./components/AEK_COM_BLEV1.h:23:31: fatal error: AEK_COM_BLEV1_cfg.h: No s...

AGUPT.1 by Associate II
  • 1596 Views
  • 1 replies
  • 0 kudos

Resolved! SPC560B60L7 microntroller compatibility with MPC5606B

Hi,I'm doing a HW rework design about a board that use the microcontroller MPC5606B of NXP. I want update the design using a ST microcontroller. I have seen that this device is similar to the SPC560B60L7, but I would like to know if the 2 IC are pin-...

how to enable JTAG in SPC56EL60?

Hello there,I want to enable/disable JTAG in SPC56EL60 microcontroller, however i did not found such information in reference manual. Could you provide clarify how can JTAG can be enabled/disabled from Sw? Thanks

Resolved! Unable to find component plugin named 'com.st.spc5.components.spc5rla.usbtypec.full.feature.feature.group 1.3.2'

I am trying to install autodevkit plugin using install new software option from help but some features are not getting installed.I am getting the following error:Missing requirement: Autodevkit feature Group 1.1.1.20200327200248 (com.st.tools.autodev...

AGUPT.1 by Associate II
  • 1788 Views
  • 1 replies
  • 0 kudos