cancel
Showing results for 
Search instead for 
Did you mean: 

struck in wait_for_transfer_completion() when I enable freeRTOS. for AEK_AUD_C1D9031.

shiva_shankar_e
Associate III

shiva_shankar_e_0-1713787970729.png

I debug up to hear and the flow of the code is blocked in this function,(after adding freeRTOS) in  the project. i don't know what is the error. i had used the low level API which is avaliable in the document. 

shiva_shankar_e_1-1713788885119.png

the flow is like this in the main function. at AEK_903D_Init(). it is blocked. and not coming out of that API. please help me out.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Max VIZZINI
ST Employee

Hi,

As I have already stated, the code has NOT be written from freeRTOS therefore it requires modification.

In particular all osalThreadDelay() are not working under freeRTOS. They have to be substituted with:

 

vTaskDelay () specifies a wake time relative to the time at which the function is called

OR

vTaskDelayUntil () specifies the absolute (exact) time at which it wishes to unblock

 

Example code:

TickType_t xLastWakeTime = xTaskGetTickCount();

vTaskDelayUntil( &xLastWakeTime, 200 );

where 200 are in milliseconds.

 

Best Regards,

AutoDevKit Team

View solution in original post

1 REPLY 1
Max VIZZINI
ST Employee

Hi,

As I have already stated, the code has NOT be written from freeRTOS therefore it requires modification.

In particular all osalThreadDelay() are not working under freeRTOS. They have to be substituted with:

 

vTaskDelay () specifies a wake time relative to the time at which the function is called

OR

vTaskDelayUntil () specifies the absolute (exact) time at which it wishes to unblock

 

Example code:

TickType_t xLastWakeTime = xTaskGetTickCount();

vTaskDelayUntil( &xLastWakeTime, 200 );

where 200 are in milliseconds.

 

Best Regards,

AutoDevKit Team

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.