AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! AEK-POW-BMS63EN voltage measurement error

Dear experts, I am facing an issue when measuring a pack of 14 batteries Fenix ARB-L18-2600. When fully charge 4.23 Volt, the BMS63EN return around 4.0x Volt. When the batteries reduce to 4.12 Volt, the BMS63EN return ~3.98 Volt. Could experts tell m...

trishuynh by Associate III
  • 4961 Views
  • 8 replies
  • 0 kudos

Resolved! AutoDevKit Studio 2.5.0 release???

 Hi at the AEKStudio 2.5.0 Release Notesit is mentioned for a while now, that the V2.5.0 is released.But at the ST Site, where the Link is (STSW-AUTODEVKIT - AutoDevKit Studio for 32-bit power architecture MCUs - STMicroelectronics)is still only the ...

THöfl.1 by Associate III
  • 2493 Views
  • 2 replies
  • 1 kudos

Resolved! Set JTAG password lock SPC58EC80E5/AEK-MCU-C4MLIT1

Hello, I'm working with the AEK-MCU-C4MLIT1 board, which features the SPC58EC80E5 MCU. While using UDE STK 5.2, I noticed that the JTAG connection is always successful, regardless of the password set to unlock it. This suggests that the JTAG password...

Johxp by Associate
  • 1881 Views
  • 1 replies
  • 0 kudos

Resolved! AEK-POW-BMS69EN Custom Battery Project

Hello, I plan to make a 333V Battery using AEK-MCU-C4MLIT1 as the master, AEKSCOM-ISOSPIA as the translator and AEK-POW-BMS69EN as the slave BMS Boards.  So far, I have been using the Example "SPC58EC—AEK_POW_BMS63EN_SOC_Estimation_Single application...

Vipuls by Associate III
  • 2385 Views
  • 1 replies
  • 0 kudos

Resolved! AEK-POW-BMS63EN Short CIrcuit on Daisy Chain

Hello Community, I have an observation from my attempt to daisy chain multiple AEK-POW-BMS63EN devices.  I have made a battery pack which has two 14-cell Battery modules in series. One module is supposed to be connected to one AEK-POW-BMS63EN and sen...

Vipuls by Associate III
  • 3830 Views
  • 4 replies
  • 2 kudos