AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CAN Transceiver usage in L99DZ200G

I've recently evaluated the AEK-MOT-MR200G1 and AEK-MOT-TK200G1 evaluation boards to gain a better understanding of using the L99DZ200G device and have noticed that neither of those boards used the on-chip CAN transceiver in the L99DZ200G device but,...

dlkeng by Associate III
  • 1809 Views
  • 1 replies
  • 1 kudos

New AutoDevKit release 2.2.1

Dear All, A bug fix release has been generated to restore at least partially the missing RLA demos. For example for the SPC58EC you can find former basic peripheral demo under SPC58EC-DISP, You can download the newest version from www.st.com/autodevk...

Resolved! Is there a charger matching BMS63EN?

I wonder if there is any ST solution on charging a batterypack that already uses the BMS63EN? So that these two could work together in terms of powercontrol. Or is it maybe easier to implement than I think? 

Orbiter by Senior
  • 2369 Views
  • 1 replies
  • 1 kudos

Resolved! The CAN example and how to properly make it work

Question 1: When I make the mcanconf like described in AN the second mcanconf is named exact the same, it does not autoincrement to mcanconf1 as it is in the example. Is that important? Or how/when do I link a certain mcanconf to a subsystem? They mu...

Orbiter by Senior
  • 4086 Views
  • 4 replies
  • 2 kudos

Resolved! Am I the only one struggeling or am I the only one using SPC?

Hi everyone!My disappointment has reached the level where I write about it. Mostly to find a way to navigate the  ecosystem or to find an alternative. My initial idea was to move from Atmel 8-bits towards something more powerful. Usecase is automotiv...

Orbiter by Senior
  • 4540 Views
  • 8 replies
  • 1 kudos

Resolved! AEK Examples Import - where to find unchanged examples

The examples are a great resource to get started. But it looks like when making changes to an example it does not only safe in the working folder. It also safes (or changes) the original. After playing a lot with one example I wanted to just delete i...

Orbiter by Senior
  • 2440 Views
  • 3 replies
  • 1 kudos

Resolved! L9963 Library for SPC5 MCU

Hi,I'm looking for C Software library for Battery Management System ST L9963.My setup:IDE: SPC5StudioMCU: SPC570SxxPlease, where can I find this library?ThanksLeo

LeoC by Associate II
  • 2726 Views
  • 3 replies
  • 2 kudos