2024-02-24 10:23 AM
Hi,
I would like to check if STM AEK-POW-BMS63EN board can be used as a first board in the daisy chain with the setup where we have external MCU (for example STMF103RB) and AEK-COM-ISOSPI1?
In the datasheet you describe difference between 'Master' and 'Slave' in the following way:
and all your AEK-POW-BMS63EN comes with SPEIN pin pull-down via R20:
Can you please clarify if the usage of AEK-POW-BMS63EN in the single BMS setup with external MCU is even possible?
BR,
MaraLo
Solved! Go to Solution.
2024-02-24 11:52 AM
hi,
Yes, for a single node you can use STM32 SPI to AEK-COM-ISOSPI1 and connect the AEK-COM-ISOSPI1 to the AEK-POW-BMS63EN.
Be careful that endianess of STM32 and SPC5 is different (big endian).
Best Regards,
AutoDevKit Team
2024-02-24 11:52 AM
hi,
Yes, for a single node you can use STM32 SPI to AEK-COM-ISOSPI1 and connect the AEK-COM-ISOSPI1 to the AEK-POW-BMS63EN.
Be careful that endianess of STM32 and SPC5 is different (big endian).
Best Regards,
AutoDevKit Team
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.