2023-08-02 12:03 AM
Dear sir,madam,
I have a questions about schematics in figure 3 of TDA7498s datasheet:
- should pin PGND (18) be left unconnected to ground?
- pin VSS (36) is also left unconnected to ground or it is on potential (VCC - 3.3 V)?
- are SUB_GND(1) and for example SGND(27) on the same potential (different symbol)?
- can be pin VDDS (26) used instead of external 3.3 V regulator (IC2)?
- what is the bias voltage on pins INPA, INNA, INPB and INNB? Is this common voltage available on any pin (maybe SVR (29))?
2023-08-08 2:30 AM - edited 2023-08-08 2:31 AM
Welcome @iloveasic, to the community!
Does it answer your questions?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.