cancel
Showing results for 
Search instead for 
Did you mean: 

Synchronous Slave SAI Sub-block Clock Source

Mohamed Jallouli_2
Associate II
Posted on July 20, 2017 at 14:13

Hello Community,

Does the SAI sub-block clock source matter when it is in Synchronous Slave mode with the other sub-block? In other words, should the two sub-blocks have the same clock source?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
bendkhilarwa
Associate III
Posted on September 23, 2017 at 21:10

Hello, 

To use two block SAI working synchronously, you need to configure the first block as an asynchronous master and the other one as a synchronous slave. Then, The two blocks will share the FS ,BCLK and MCLK lines. And each one will have its own data line.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.