2023-11-13 9:06 AM
Dear Sirs!
I use in my design LMV321LICT manufactured by STMicroelectronics. And I faced very strange behavior.
LMV321LICT powered by +3V in mode of buffer or non inverting amplifier.
When for example there is +1.5V DC in plus input and gain 2, I see about +3V in output (no load).. It really work as rail to rail amplifier as expected.
But when there is +3V DC in plus input and gain 1, I see about +2.5 V on output (no load) but I expected to see +3V.
I have not found in datasheet any limitations about input voltage.
Can you please explain?
Is it a correct behavior for this amplifier or something wrong in my board?
Best regards
Michael
Solved! Go to Solution.
2023-11-13 9:42 AM - edited 2023-11-13 9:44 AM
is as in ds : max. input Vcc-1V ; so at 3V vcc max. 2V at input.
+ if you want input range 0..vcc , need R2R input and output opamp !
2023-11-13 9:42 AM - edited 2023-11-13 9:44 AM
is as in ds : max. input Vcc-1V ; so at 3V vcc max. 2V at input.
+ if you want input range 0..vcc , need R2R input and output opamp !
2023-11-13 10:43 AM
You can find the information mentioned by the above answerer in paragraph 4.2 in the datasheet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.