2019-11-08 5:14 AM
Hello,
i try for moths to get a wave file from SD to the DAC.
I the ST LL_DAC_ADC_project description stands.
#############################################
LL_DAC_EnableDMAReq(DAC1, LL_DAC_CHANNEL_1); // enable DMA for Channel1
LL_DAC_Enable(DAC1, LL_DAC_CHANNEL_1); //enable Channel on DAC
LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_7 , (uint32_t)dacbuf, LL_DAC_DMA_GetRegAddr(DAC1, LL_DAC_CHANNEL_1, LL_DAC_DMA_REG_DATA_12BITS_RIGHT_ALIGNED ), LL_DMA_DIRECTION_MEMORY_TO_PERIPH );
LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_7, DACBUFSIZE );
LL_DMA_EnableDoubleBufferMode(DMA1, LL_DMA_CHANNEL_7);
LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_7); // This command is not existing
#############################################
I try it on my own with this startup
#############################################
LL_DAC_EnableDMAReq(DAC1, LL_DAC_CHANNEL_1); // enable DMA for Channel1
LL_DAC_Enable(DAC1, LL_DAC_CHANNEL_1); //enable Channel on DAC
LL_DMA_ConfigAddresses(DMA1, LL_DMA_STREAM_5 , (uint32_t)&DAC_Buff, LL_DAC_DMA_GetRegAddr(DAC1, LL_DAC_CHANNEL_1, LL_DAC_DMA_REG_DATA_12BITS_RIGHT_ALIGNED ), LL_DMA_DIRECTION_MEMORY_TO_PERIPH );
LL_DMA_SetDataLength(DMA1, LL_DMA_STREAM_5, DACBUFSIZE );
LL_DMA_EnableStream(DMA1, LL_DMA_STREAM_5);
LL_DMA_EnableIT_HT(DMA1, LL_DMA_STREAM_5);
LL_DMA_EnableIT_TC(DMA1, LL_DMA_STREAM_5 );
#############################################
It compiles correct but in my function the interrupt never happens
char wave_playback(const char *FileName)
{
FRESULT res;
FIL file;
UINT cnt;
res = f_open( &file, FileName, FA_READ );
if(res) return 1;
res = f_lseek(&file,0x2c);
if(res) return 2;
f_read (&file,&DAC_Buff[0],512,&cnt);
if(res) return 3;
TIM6->CR1 |= TIM_CR1_CEN;
while(1)
{
volatile ITStatus it_st;
it_st = RESET;
while(it_st == RESET) {
it_st = LL_DMA_IsActiveFlag_HT5(DMA1);
}
f_read (&file,&DAC_Buff[0],256,&cnt);
LL_DMA_ClearFlag_HT5(DMA1);
//DMA_ClearFlag(DMA1_Stream5, DMA_FLAG_HTIF5);
//ToDo clear all flags in the DMA_LIFCR and DMA_HIFCR registers before starting a new transfer
if(cnt<256)break;
it_st = RESET;
while(it_st == RESET) {
it_st = LL_DMA_IsActiveFlag_TC5(DMA1);
}
f_read (&file,&DAC_Buff[256],256,&cnt);
LL_DMA_ClearFlag_TC5(DMA1);
if(cnt<256)break;
}
TIM6->CR1 &= ~TIM_CR1_CEN;
f_close(&file);
return 0;
}
Timer Settings are:
####################################################
static void MX_DAC_Init(void)
{
/* USER CODE BEGIN DAC_Init 0 */
/* USER CODE END DAC_Init 0 */
LL_DAC_InitTypeDef DAC_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_DAC1);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
/**DAC GPIO Configuration
PA4 ------> DAC_OUT1
PA5 ------> DAC_OUT2
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_4|LL_GPIO_PIN_5;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* DAC DMA Init */
/* DAC1 Init */
LL_DMA_SetChannelSelection(DMA1, LL_DMA_STREAM_5, LL_DMA_CHANNEL_7);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_STREAM_5, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetStreamPriorityLevel(DMA1, LL_DMA_STREAM_5, LL_DMA_PRIORITY_LOW);
LL_DMA_SetMode(DMA1, LL_DMA_STREAM_5, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_STREAM_5, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_STREAM_5, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_STREAM_5, LL_DMA_PDATAALIGN_HALFWORD);
LL_DMA_SetMemorySize(DMA1, LL_DMA_STREAM_5, LL_DMA_MDATAALIGN_HALFWORD);
LL_DMA_DisableFifoMode(DMA1, LL_DMA_STREAM_5);
/* DAC2 Init */
LL_DMA_SetChannelSelection(DMA1, LL_DMA_STREAM_6, LL_DMA_CHANNEL_7);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_STREAM_6, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetStreamPriorityLevel(DMA1, LL_DMA_STREAM_6, LL_DMA_PRIORITY_LOW);
LL_DMA_SetMode(DMA1, LL_DMA_STREAM_6, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_STREAM_6, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_STREAM_6, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_STREAM_6, LL_DMA_PDATAALIGN_HALFWORD);
LL_DMA_SetMemorySize(DMA1, LL_DMA_STREAM_6, LL_DMA_MDATAALIGN_HALFWORD);
LL_DMA_DisableFifoMode(DMA1, LL_DMA_STREAM_6);
/* USER CODE BEGIN DAC_Init 1 */
// LL_DMA_SetMemory1Address(DMA1, LL_DMA_STREAM_5, (uint32_t)&DAC_Buff);
//LL_DMA_SetPeriphAddress(DMA1, LL_DMA_STREAM_5, (uint32_t)(DAC_BASE + 0x10));
/* USER CODE END DAC_Init 1 */
/** DAC channel OUT1 config
*/
DAC_InitStruct.TriggerSource = LL_DAC_TRIG_EXT_TIM6_TRGO;
DAC_InitStruct.WaveAutoGeneration = LL_DAC_WAVE_AUTO_GENERATION_NONE;
DAC_InitStruct.OutputBuffer = LL_DAC_OUTPUT_BUFFER_ENABLE;
LL_DAC_Init(DAC, LL_DAC_CHANNEL_1, &DAC_InitStruct);
/** DAC channel OUT2 config
*/
LL_DAC_Init(DAC, LL_DAC_CHANNEL_2, &DAC_InitStruct);
/* USER CODE BEGIN DAC_Init 2 */
/* USER CODE END DAC_Init 2 */
}
####################################################
Does anybody knows what to do because I am coplitly lost at this point.
2020-06-23 5:38 AM
Hello,
this post is a bit old, so in case you haven't solved yet, you missed the TRIG enabler:
LL_DAC_EnableTrigger(DAC, LL_DAC_CHANNEL_1);
LL_DAC_EnableTrigger(DAC, LL_DAC_CHANNEL_2);I hope tihs help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.