2015-04-16 1:36 AM
Hi,
I've bought ''steval-mki126v1'' and ''steval-mki138v1'' evaluation boards (and ''Microphone Coupon Board steval-mki129v1'') . My goal is only to RECORD the signals coming to each microphone/channel (produce a WAV files). 1) When I use APWorkbench on ''steval-mki138v1'', try to record (pressing on ''start''), the next pop-up message shows: mmioOpen:- 2147467259, prevent me to produce the WAV files. 2) Using APWorkbench on ''steval-mki129v1'' (via steval-mki138v1 and USB connector), don't give option to capture/record any channel to audio file, how can I get those data? Thanks a lot David2015-04-19 1:20 AM
someone?
does this forum Active??2015-04-20 8:38 AM
Hi David,
The APWorkbench allows to record live streams from the MEMS microphones mounted on the STAudioHub interface - through the ''USB Digital Voice Recorder'' panel. Is it this one that you're selecting in your below case-1 and producing the mmioOpen error? Marco2015-04-27 4:41 AM
Dear Marco,
I've tried to explain clearly our team problems, Please see the attached file, Thanks! David ________________ Attachments : ST_Problems.docx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Ht1j&d=%2Fa%2F0X0000000aIy%2FUpkwbnHfZq62vDW7NO3dHi1yNsk8OAw2MRfXw.JfOAQ&asPdf=false2016-10-28 2:08 AM
Hi,
I also have the same issue as David. In addition, when i try to play the sound that is recorded, although it plays it on screen visually, it does not give any sound output. Is there a solution to this?Kind regards,FatihWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.