2021-09-14 3:28 AM
2021-09-14 8:19 AM
Is there a question here? You can write to FLASH in your program using the various HAL_FLASH_* calls. There should be examples in the relevant CubeMX repository for your chip.
2021-09-14 9:53 AM
Do you plan on writing the Windows side application replacing the ST-LINK Utility?
How do you propose to do the download? Via serial? Using X/Y-MODEM type protocol?
You can implement the target side code via the HAL Flash calls to erase and write to the memory area to be used for the binary data.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.