Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

TSV632 - negative input current allowed?

Posted on June 27, 2013 at 11:53Hello,the datasheet for the OpAmp TSV632 allows a maximum input current of 10mA (page 4).There's no sign given, so I suppose negative input currents aren't allowed.. But I'm not sure and it would help me, if they woul...

Offline opamps catalog ?

Posted on June 18, 2013 at 11:23Hello, I'm product engineer and I'm regularly looking for op-amps on the your website. Having a slow connection, I'm looking for a way to select op-amp being offline. Do you have somthing to help me ? Thanks, Allan ...

allan by Associate
  • 1877 Views
  • 2 replies
  • 0 kudos

STA326 Thermal Pad is GND?

Posted on June 06, 2013 at 03:39Is the STA326 thermal pad connected to GND/SUBGND or floating? Something happened when I installed a heatsink on the STA326 that caused 30V VCC to appear on the 3.3V VDD side, destroying all other components on my boa...

stv7302a

Posted on May 16, 2013 at 17:01buen día, por favor necesito ayuda para obtener, the datasheet  for stv7302a  

TDA7375V current limiter?

Posted on December 23, 2012 at 23:13Good night,I've mounted a TDA7375V power amplifier on a breadboard with a 3ºC/W heatsink, and with a 16.5V/4A power suplly, the amplifier is in bridge configuration and driving 6 ohm speakers, the circuit is simi...

TDA7297 and TDA2822M with the same supply

Posted on December 24, 2012 at 18:14Good afternoon,I've mounted 2 amplifiers using the same power supply using 3 breadboards, one is for a TDA7297 power amplifier which is running perfectly with some changes to the specified circuit, like 470nF inpu...

TDA2822M RF interference

Posted on December 23, 2012 at 23:17Good night,I'm using a TDA2822M to drive headphones in a breadboard prototype, but the problem is the amplifier that captures every RF interference such that of power switches and electric engines.Could this be a ...

TSC888A gain is low

Posted on January 02, 2013 at 19:50I'm using the TSC888A current sensing amplifier in BLDC (brushless DC) motor controller current limit circuit. I'm seeing a gain of about 10 from the amplifier instead of the published typical value of 20. The data...

Noise Analysis and SPICE Model for TS9224

Posted on August 01, 2012 at 21:19Hi,I am working on an instrumentation amplifier circuit.  I would like to perform a noise analysis on the circuit and would like to get a SPICE model for the TS9224 opamp.  I am using LTSpice.  I could also use some...

Quiescent current definition

Posted on June 11, 2012 at 15:45What is the definition of quiescent current parameters in operational amplifier project? Thanks, Luli #quiscent-current

luli755 by Associate
  • 1501 Views
  • 1 replies
  • 0 kudos