cancel
Showing results for 
Search instead for 
Did you mean: 

STA326 Thermal Pad is GND?

bmclaughlin10
Associate
Posted on June 06, 2013 at 03:39

Is the STA326 thermal pad connected to GND/SUBGND or floating?

Something happened when I installed a heatsink on the STA326 that caused 30V VCC to appear on the 3.3V VDD side, destroying all other components on my board. It seemed to happen right when I connected the STA326 heatsink to my PCB ground plane with screws.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
bosco.stefano
ST Employee
Posted on June 10, 2013 at 10:32

The thermal pad is connected to pin GND SUB (pin 1) and can be either left floating or connected to GND.

The only hyoptesis about the problem you are facing is a mechanical short between metallic heatsink and Vcc/Vdd.

Verify the assembly of heatsink and components near it (e.g. decoupling capacitor).

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.