Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

tda 7560 ic not working problem

I bought this chip and pcb circuit from the internet, then when I plugged all the components into the pc and powered it up, I couldn't get any sound. When I powered up the circuit, it got hot inside, but only a low sound came from one speaker pin, bu...

FicoresS by Associate II
  • 5355 Views
  • 6 replies
  • 0 kudos

Change TDA7808 for TDA7803

Hi. I bought a multimedia screen for my car that I wanted with the TDA7803 chip, but the seller sent me a unit with the TDA7808 chip. I'm noticing that the chip is getting too hot. I am using speaker system with less than 4 ohms. That's why I wanted ...

Resolved! Identifying an ST chip

I am currently working on repairing a Taramps MD3000.1 car amplifier. There is an ST chip with the following markings: 319MZLBD38 or it could be MZLB038.I'm not sure what it is and am having quite a time finding that out. I appreciate any feedback!

EMI issues with the TDA7492E

Hello -We are having issues with EMC compliance with the TDA7492E. We have broadband radiated EMI between 100MHz and 200MHz that is above the limits. I've included a screenshot of the testing lab's report with the radiation. I've attached our schemat...

jasong by Associate II
  • 7565 Views
  • 6 replies
  • 1 kudos

Resolved! Laney LA65C, TDA7294

Hello, I have a guitar amp Laney LA65C where the output amp is faulty, it consists of a TDA7294 IC, I put in a new TDA7294 but it exploded as soon as the power was turned on. I checked the input voltage and it is correct 26 volts, what could cause it...

Lopo1132 by Associate
  • 4347 Views
  • 2 replies
  • 2 kudos

Signal conditioning for NDIR sensor

I am wondering why they use a thermistor to monitor temperature when they have a reference detector?https://www.st.com/resource/en/application_note/an5571-signal-conditioning-for-ndir-sensor-stmicroelectronics.pdf  

spi receives mp34dt05pdm data

我现在想用stm32F407系列的spi口来采集mp34dt05的PDM麦克风的数据,但是我发现我采集到的pdm数据流基本上不会因为我的环境变化而产生任何变化。你能详细告诉我spi是怎样的吗?要接收mp34dt05的数据,麦克风芯片mp34dt05有驱动文件吗?如果有的话可以发给我吗?感谢您的关注。Translated from Chinese to English: I am now trying to use the spi port of the stm32F407 series to c...

Daqiang by Associate II
  • 1162 Views
  • 0 replies
  • 0 kudos

Resolved! Assistance indentifying component - ZKW diode

Hello, I am attempting to identify a component from a switch mode power supply out of a audio preamp.I am 90% confident it is a zener diode, but after that I am at a loss. Markings (cathode band on left):(ST) 98ZKW  *not sure if there is a space betw...

rdenbroe by Associate
  • 2471 Views
  • 1 replies
  • 2 kudos