Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

TSV791/2 Output Impedance

Hello, I am interested in using theTSV791/2 for ADC driver and reference buffer purposes.The reference buffer needs to both source AND sink significant amounts of current (mA) and I am interested in the amplifier's transient response.I did not see an...

KYin.2 by Associate II
  • 882 Views
  • 0 replies
  • 0 kudos

AUDIO_OUTPUT_BUFF_SIZE Bit mismatch while separating audio data from 4 channels TDM data. (Audio data extraction and processing on AMicArray_Microphones_Streaming demo example)

I have been studying the x-cube-memsmic1's AMicArray_Microphones_Streaming example. I have used 4 channel mic array expansion module. As per the theory, incoming data is from 4 channels, 16-bit slot size per channel, and 96khz sampling frequency. so...

PJ.3 by Associate
  • 731 Views
  • 0 replies
  • 0 kudos

No output on TDA7498MV

Hello, I'm having problems with the circuit using TDA7498MV. I have made a PCB as recommended in the datasheet. I have connected 3v3 to MUTE and STBY pins, and a power supply of 30V to power pins.On the VDDS pin I get an output of 3v3 and on SYNC LK ...

AKonc.1 by Associate
  • 826 Views
  • 0 replies
  • 0 kudos

Resolved! I would like to use STuW81300 on my device but I don't ensure how to design Internal LDO output. I need to help.

When I read the STuW81300 datasheet, I learned to need to use 10uF and small resistance at the output of LDO. I will share the Application Diagram below this. But when I read the UM2218 User manual, I saw the bellow figure.I don't know if I need that...

0693W00000KdjMeQAJ.png 0693W00000KdjWAQAZ.png