2024-09-13 9:34 PM
Hi, thank you for having access to this report.
Here is STM32CubeProgrammer's output text.
(0) > STM32_Programmer_CLI --connect port=swd -w .\board\art-pi\projects\applications\build\Debug\applications.elf 0x90000000 -v -el .\board\art-pi\ExternalLoader\ART-Pi_W25Q64.stldr
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
ST-LINK SN : 066BFF554957886687101038
ST-LINK FW : V2J42M27
Board : --
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x91
Warning: Write address is ignored for hex, Srec, s19 and elf files
Memory Programming ...
Opening and parsing file: applications.elf
File : applications.elf
Size : 996.35 KB
Address : 0x90000000
Erasing memory corresponding to segment 0:
Erasing external memory sectors [0 249]
Download in Progress:
��������������������������������������������������� 100%
File download complete
Time elapsed during download operation: 00:00:11.568
Verifying ...
Read progress:
��������������������������������������������������� 100%
Download verified successfullyThis works fine, but he doesn't feel very well.
And I tried to use utf-8 encoding format, but it's still garbled.
2025-02-20 3:24 AM
Hi,Aziz
I've seen a lot Chinese users met that garbled character problem in other forums. Cause Vscode terminal is UTF8 by default and encoding 850 or 437 is rarely used in Asia. I change my local STM32VSCODE extension file, adding chcp 437 &&(or chcp 850 &&) right before STM32CubeProgrammerCLI command in "flash" task template, and that just fix mine. To get a better performance in more computers, is it feasible to add that "chcp 437" or "chcp 850" to extension's source code?
Thanks in advance!
2025-04-05 10:03 PM
This has nothing to do with VSCODE, the problem is on Windows Terminal. As mentioned earlier, I changed the code page to 850 before using the STM32ProgrammerCLI. Today I tried to active code page to 437, but the result is still the same.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.