2025-03-19 3:26 AM
My company wishes to implement a feature in an existing C# application in order to download firmware to MCUs (USB DFU only).
I was able to get this done using the drivers and dlls provided through Dfuse (https://www.st.com/en/development-tools/stsw-stm32080.html).
There seems to be an issue concering the Dfuse driver on some of our computers which is why I tried to do the same using the driver and the CubeProgrammer_API.dll which are both part of the STM32CubeProgrammer (https://www.st.com/en/development-tools/stm32cubeprog.html). I managed to get that working as well, but it seems like the CubeProgrammer_API.dll needs a lot of other files to be able to work (>400MB).
This is why I was wondering if the CubeProgrammer_API.dll accesses another separat dll that only handles the USB DFU protocol (like STDFU.dll which is part of Dfuse) and does not need the >400MB of files.
Best,
Stefan
Solved! Go to Solution.
2025-04-25 7:46 AM
Hello @SMeier,
You can checkout STM32CubeCLT available under this link
The STM32CubeProgrammer package inside it will support all programming interfaces and is ~90 MBs.
Aziz
2025-03-19 4:08 AM
You can try dfu-util instead. It is an open-source DFU tool that supports STM32. This could be wrapped in C# via process execution.
2025-04-25 7:46 AM
Hello @SMeier,
You can checkout STM32CubeCLT available under this link
The STM32CubeProgrammer package inside it will support all programming interfaces and is ~90 MBs.
Aziz
2025-04-25 2:56 PM
The (kernel) driver behind the DFU mode is simply the winusb. It is standard in-box Windows component, the only hitch is "installing" it, that's, associating it with specific USB device IDs.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.