2026-02-12 4:19 PM
I am having to program a unit via UART, and every time I open the STM32CubeProgrmmer GUI the interface selector shows J-Link/Flasher.
It remembers if I choose ST-Link.
If I manually edit the "interface=" entry in config.properties to 2, STM32CubeProgrmmer opens with UART selected.
On exit, the "interface=" entry is rewritten to 1.
If I select USB as the interface, the "interface=" entry is rewritten to 2, which opens as UART the next time, and then the "interface=" entry is rewritten to 1 on the next exit.
2026-02-17 8:09 AM
Hello @LurkingKiwi,
Thank you for reporting this. I have submitted a ticket to our team for resolution.
Internal ticket number: 227481 (This is an internal tracking number and is not accessible or usable by customers).
Thanks,
Amine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.