2022-07-20 2:48 AM
Dear all
Under windows 11 the 64 bit setup (2.11) starts
with extracting the file and after that I see sometimes the busy signal, but
...
There are no entries in the windows event logger.
I know, that windows 11 isn’t mentioned in the release notes (RN0109).
Can I start the setup with command line parameters?
Thanks in advance,
Franz
2023-08-18 9:02 AM
The problem still exists with version 2.14.0.
Any assistance would be greatly appreciated.
2023-08-18 11:37 AM
@FWege.1 What are the missing entries in the Windows event logger? What exactly is the problem? What is the "but..." ?
2023-08-18 3:03 PM
Hello Pavel A.
First - thanks for your answer!
After double clicking the setup file the blue circle (appearing next to the mouse pointer) blinks.
I suppose this indicates some background activity.
Nothing further happens.
The task manager shows 2 processes.
No entry in the windows event log which indicates an error.
Firewall was disabled. Run as administrator was done.
Other installations run as expected.
2023-08-19 4:02 AM
This is strange, we have installed previous STM32CubeProgrammer versions on Win11 x64 several times and it works well.
Windows is a complex environment with possible presence of 3rd party software and hardware. Troubleshoot as usual for such issues.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.