2020-05-31 6:06 PM
[ The text uses a translation tool. ]
Flash size is the default and no more programs can be loaded.
environment
Windows10 + STM32CubeMX + ST-Link2
************** Console log
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 53FF6D064882505226101587
ST-LINK FW : V2J36S7
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x436
Device name : STM32L15xxD/STM32L162xD
Flash size : 128 KBytes (default)
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a20796.srec
File : ST-LINK_GDB_server_a20796.srec
Size : 137888 Bytes
Address : 0x08010000
Erasing memory corresponding to segment 0:
Error: Operation exceeds memory limits
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
*************
I'm using an STM2L151DTx, so there's plenty of flush
Why is it [Flash size: 128 KBytes (default)]?
The STM32 ST-LINK Utility can be recognized and written normally.
Am I doing something wrong?
2021-09-20 10:36 AM
Continues to be broken.. Another report for the STM32L15x family
2021-09-22 7:37 AM
WHEN WILL YOU FIX THIS ISSUE????????????????????????????????
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.