2024-07-25 1:05 AM - edited 2024-07-25 1:09 AM
Hi,
We are using STM32_Programmer_CLI on windows and linux.
I noticed that since version 2.16 following commands fails:
STM32_Programmer_CLI -c port=SWD freq=8000 sn=x mode=UR -e ed1 & ed2
with:
Error: The erase command you trying to perform is missing some arguments. Please refer to the Help to see how to use it.
It worked fine on version 2.15. I've looked into any api changes for newer version in release notes but I couldn't find any relevant changes that could affect this behavior. For me, it looks like this is potential bug/regression. Let me know if me guess is correct or we need to adjust params added to command.
Thx
Solved! Go to Solution.
2024-12-05 4:34 AM
Hello,
The problem has been resolved in STM32CubeProgrammer v2.18.0
You can download it from this Link.
Maryem.
2024-07-29 2:32 AM
Hello @pwl,
Yes, you are correct. This is a known issue related to erasing EEPROM sectors, and it is currently under investigation by our development team.
Internal ticket number: 186569 (This is an internal tracking number and is not accessible or usable by customers).
I'll keep you updated.
Thanks,
Amine.
2024-10-30 12:06 PM
Hi,
Is there a workaround or solution available or status on being fixed in version 2.18?
Thanks!
2024-10-31 9:21 AM
Hello @rload,
The fix will be included in the future release of CubeProgrammer. In the meantime, you can try using the GUI of version 2.17.0 or the CLI of version 2.15.0. I'll keep you posted. Thank you for your understanding!
Maryem.
2024-12-05 4:34 AM
Hello,
The problem has been resolved in STM32CubeProgrammer v2.18.0
You can download it from this Link.
Maryem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.