2019-11-09 12:11 AM
Hi, I am trying to use Stm32 cube programmer with stm32h753 in USB dfu mode. Moving the mcu in boot loader mode and usb is appearing , when I press the connect button it gives this error
23:42:46:012 : Error: Data read failed
23:42:46:170 : Warning: Connection to device 0x450 is lost
I did run dfu with other mcu stm32l4 successfully but I am not able to run it with stm32h753 .
Any advise? Did any one run cube programmer with this mcu?
Thanks,
2019-11-09 4:15 PM
Do you use the latest Cube programmer version?
2019-11-09 7:24 PM
Yes.
2019-11-10 8:03 AM
>> Did any one run cube programmer with this mcu?
Used them in assorted H7 micro-controllers, mainly use SWD for debugging, not DFU/USB
USB would have dependency on HSE clock, I'd hope AN2606 would provide specific details.
2019-11-10 8:57 AM
Hi Clive,
Is not responsibility of stm system bootloader setting HSe .As when mcu goes in bootloader mode then user application clocks setting may not be effective.
2019-11-10 9:30 AM
ST claims (AN2606) to be using HSI48 to drive the USB peripheral. CRS I assume qualifies the local clock against the signaling from the host.
If this is a custom board I would probably look at the power supply, and VCAP caps/voltages. Perhaps scope/trigger on NRST to see if that can be attributed to the drop of a USB/DFU connection.
Likely going to need to make a more compelling case to gain interest from ST to address/identify issues with STM32 Cube Programmer.
My use cases tend to use JTAG/SWD and USART methods.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.