2025-08-09 11:14 PM
The CLI works fine on Windows 10 but on a Windows 11 computer I get this output:
Unlock Success
Patched SREC with unique ID
STM32 ST-LINK CLI v3.6.0.0
STM32 ST-LINK Command Line Interface
ST-LINK SN: 62021102220032524B413836
ST-LINK Firmware version: V2J37S7
Connected via SWD.
SWD Frequency = 4000K.
Target voltage = 3.3 V
Connection mode: Normal
Reset mode: Hardware reset
Device ID: 0x418
Device flash Size: 128 Kbytes
Device family: STM32F10xx Connectivity Line
Loading file...
Unable to open file!
It would be really helpful if the error message gave the path of the file it can't open.
2025-08-10 6:29 AM
What arguments are you calling the CLI with? Spaces in path?
2025-08-10 6:41 AM
I'm not calling it, it's called by a flashing app. The same app that works perfectly on Windows 10.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.