2020-11-11 4:58 AM
I'm using STMCubeProgrammer for program STM32F103 MCU. But I don't have any access to MCU RESET PIN. So I enter to BOOT Mode by source code in my application, But when I want to turn back to application from boot mode the "Run After Programming" option doesn't work correctly.
How can I turn back to application from boot mode without access to reset Pin?
Thanks.
2020-11-11 5:59 AM
Bootloaders knows a "go <address>" command. But why not reset the MCU programmatically? To make option byte setting actiive, either option byte reload or reset is needed anyways.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.