2024-09-10 7:28 AM
STM32CubeProgrammer version 2.17.0
Target STM32G491, device ID 0x0479, 512KB flash
When loading a large hex file (284kB), the programmer tries to erase 65293 sectors! There's only 256 sectors in target, and the image only needs 141 sectors erased.
We also use the internal flash to storage some settings of the device. These settings are erased when using version 2.17.
We tried this earlier with version 2.13 and no problem was detected.
See attached log files of both version 2.13 and 2.17
Please provide help.
Thanks,
EG
2024-09-10 7:47 AM
Hello @EG1 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Could you please add the .hex file that you have been using so we can test it.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-10 8:12 AM
Dear STTwo-32,
I send you a private message with the hex file. I prefer not to place the hex file in a public location.
Please let me know if you find something.
Thanks,
EG
2024-09-12 2:04 AM - edited 2024-09-12 3:14 AM
Hello @EG1
Sorry for my late replay. I've been able to reproduce that issue, and I've escalated internally for correction on the coming releases (under internal ticket number 190918). Thank you so much for escalating.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-02 12:59 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.