2018-10-02 2:14 AM
Hi,
I just can see a flash of CubProgrammer when I double click its short-cut icon. I have re-installed it several times. It always can give me a flash.
My OS is windows 10 and JAVA version is JRE 8. The java environment setting is
Path: C:\Program Files\Java\jre1.8.0_181
JAVA_HME = C:\Program Files\Java\jre1.8.0_181
The returned information of java -version is
java version "1.8.0_181"
Java(TM) SE Runtime Environment (build 1.8.0_181-b13)
Java HotSpot(TM) 64-Bit Server VM (build 25.181-b13, mixed mode)
Thank you for your helping.
Best Regards,
Allen
2018-10-02 4:17 AM
Hi All,
I find the root cause. It installs at JKD 11 when I install CubeProgrammer first time. But It still installs at JDK 11 after I install JRE 8 and set the path and JAVA_HOME for JRE8. It works well after I remove JDK11
2018-10-10 8:49 AM
I confirm I had JDK10.2 installed and was unable to launch STM32CubeProgrammer v1.2..
Thanks for your post.
Bertrand
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.