2023-03-13 10:54 PM
we installed an application binary on NUCLEO-144/F429ZI with UART2 as an external interface and USB-UART for debugger.
And the binary code been downloaded via the debugger port using STM32CubeProgramer with the tool option of "STM32CubeProgramer(SWD)" and "USB support(if possible): None"
It goes well without readout protection of OB(Option Byte). Also well in serial out on USB-USART.
By the way, once Read out protection was set to 'BB' from 'AA', it will not go well. no output on USB-UART.
What's my misunderstanding on the Readout protection?
Solved! Go to Solution.
2023-03-15 5:57 AM
Hello @DAhn.1 ,
Thanks for the clarification,
After setting RDP to "BB", the device requires a Power OFF/ Power ON to re-start the application. Please try to unplug your board after setting RDP and then re-connect it.
Let me know if this helps!
Sara.
2023-03-14 8:49 AM
Hello @DAhn.1 ,
Thanks for your feedback,
To avoid any misundrestanding, let me share with you my comprehension: Are you trying to load a binary file on your board when Readout protection is set to BB and the device is connected via STLink?
If not could you please clarify more the issue ?
Sara.
2023-03-14 7:10 PM
Thanks for your reply.
I loaded a binary first on my board and verified its work well.
This means that a hyper terminal linked to debugger port shows the text message what I want to print.
And then I set readout protection to "BB" in OB(option byte).
After the protection set to "BB", no message responses displayed on the terminal,
DAhn.
2023-03-14 8:56 PM
When you change RDP from BB (level 1) to AA (level 0), your program gets erased and cannot print anything. This is the normal expected behavior.
2023-03-15 5:57 AM
Hello @DAhn.1 ,
Thanks for the clarification,
After setting RDP to "BB", the device requires a Power OFF/ Power ON to re-start the application. Please try to unplug your board after setting RDP and then re-connect it.
Let me know if this helps!
Sara.
2023-03-15 11:42 PM
It's OK and solved my problem with your advice.
So far I reset using only reset button on the board.
that's my problem.
Thank you again. Sara.
DAhn.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.