2025-07-30 7:36 AM - last edited on 2025-07-30 9:36 AM by Imen.D
Hi.
I am developing a bootlaoder Code by using STM32U073MCT6.
when ı am using code protection code which is below, RDP is becoming BB however, after this process, when I turn on back protection (AA) I get an error when doing a full chip erase. it says Mass erase operation failed. Please verify flash operation.
protection code
void ReadProtection(void)
{
FLASH_OBProgramInitTypeDef obConfig;
// Clear all FLASH flags
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_WRPERR | FLASH_FLAG_PGERR | FLASH_FLAG_BSY);
HAL_FLASHEx_OBGetConfig(&obConfig);
if (obConfig.RDPLevel == OB_RDP_LEVEL_0)
{
// this is first time we run mcu after flashing firmware
obConfig.RDPLevel = OB_RDP_LEVEL_1;
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
HAL_FLASHEx_OBProgram(&obConfig);
HAL_FLASH_OB_Launch();
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
}
}
Edited by ST Moderator to apply source code formatting - Please follow the recommendation in this article How to insert source code
2025-07-30 9:29 AM
So the code posted works as expected?
> when I turn on back protection (AA) I get an error when doing a full chip erase
How are you doing this? Show the error.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.