2025-12-14 11:33 AM
Hello,
I have the issue that the FlashLoader is detected but not set correctly. The error message is:
flash loader cannot be loaded. FlashLoaderPath = CubeProgrammer/bin/FlashLoader/0x
As a workaround I can create a copy of the correct FlashLoader and name it 0x, but I think this should work automatically. I am running on Linux and the issue exists for several versions of CubeProgrammer and on multiple Linux distros for me. My current version 2.21.0.
The issue is really annoying if you switch boards and forget to copy-rename the correct FlashLoader.
Solved! Go to Solution.
2026-02-24 5:42 AM
2025-12-19 12:49 AM - edited 2025-12-22 6:45 AM
Hello there Tachyon,
Thank you for reporting this issue.
We have reproduced this error and we'll report this to the dedicated team (internal ticket number: 224132).
For now, you can use the workaround and we'll let you know ASAP when this is fixed.
Furthermore, can you provide us with the Linux distributions that have caused this error, that would be of great help.
PS: Ticket number: 224132 is an internal tracking number and is not accessible or usable by customers.
Kouthair
2025-12-19 8:57 AM
One was on Linux Mint 22.1 the other on CachyOS (Arch) . Both with a german locale.
Best regards.
2026-02-24 5:42 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.