2019-12-16 7:24 AM
Hi,
we have troubles during flashing a STM32F446 with STM32CubeProgrammer 2.2.1 via SPI.
Every time the Cube Programmer wants to erase the "big" Sector 5 (128 kB) an timout error occurs. (see log file)
Everything works fine with a Hex-File except the "big" (128 kB) sectors 5 to 7 !
Is this a known bug or have we done anything wrong?
13:09:30:674 : Erasing Segment Address Size Bytes
13:09:30:674 : Erasing memory corresponding to segment 6:
13:09:30:674 : Erasing internal memory sectors [4 5]
13:09:30:674 : s 1 byte(s): 0x5A
13:09:30:694 : s 1 byte(s): 0x44
13:09:30:708 : s 1 byte(s): 0xBB
13:09:30:708 : ACK received
13:09:30:708 : s 3 byte(s): 0x00 0x02 0x02
13:09:30:708 : ACK received
13:09:30:708 : s 5 byte(s): 0x00 0x04 0x00 0x05 0x01
13:09:32:690 : Timeout error!
13:09:32:690 : Error: failed to erase memory
Best Regards,
Simon Ax
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.