2024-07-18 9:57 AM - edited 2024-07-18 10:01 AM
A write of size 294KB to STM32H7A3VGHx Internal Flash works, but a write of size 775KB does NOT
BTW, same issue with STM32CubeProgrammer v2.16.0
Solved! Go to Solution.
2024-07-18 10:26 AM
Why does in say 0x080F0000 as the Address? That's like 64KB short of the 1MB ceiling, which is WHY it's failing.
Is this a .HEX or .ELF type file internally?
2024-07-18 10:26 AM
Why does in say 0x080F0000 as the Address? That's like 64KB short of the 1MB ceiling, which is WHY it's failing.
Is this a .HEX or .ELF type file internally?
2024-07-18 11:12 AM
Internally it is a compressed binary file
The file size 294KB works, while 775KB does NOT
Further research shows that the STM32H7A3VGHx seems to have only 1MB of Internal Flash
So, starting from 0x0807-0000 there probably is only 512KB available after 0x080F-0000
If true, that will explain why 294KB works, and 775KB does NOT
Let me look at this more...
2024-07-18 11:39 AM - edited 2024-07-18 11:40 AM
Right. On VG you have not continuous memory...so flash complies about it.
BUT you could make project with H7A3VI type, 2MB flash, continuous.
(And probably you have same die - same chip, just not tested and "payed for" memory. )
So try with "VI" setting, then it should work.
+
If you need room for big program, net time buy VI version. :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.