2024-11-13 7:14 AM
Hi,
I've tried to program OTP area of STM32U575 at address 0x0BFA0010 with a quad-word (4x32bit of data) but only half are programmed (the first half) while the 2 remaining words are at 0xFFFFFFFF (erased state) and cannot be programmed anymore.
I've loaded a binary file with 128bits of data, chose the download attress at 0x0BFA0010 and pushed the download button.
Accoding to the datasheet the flash must be programmed 128bit at once: is that implemented in the programmer?
Best regards,
Diego
2024-11-13 10:24 AM - edited 2024-11-14 2:51 AM
Hello @DMoim.1
I'm checking internally this issue (tracked via internal ticket: 196262)
We will keep you updated here when progress is made in this request.
Thank you for your contribution.
2024-11-14 2:56 AM
Hi @DMoim.1
Issue is confirmed and our Dev team are working to resolve it.
In the meantime, you can try using Cubeprogrammer version 2.15.0.
Thank you for your contribution.
2025-03-07 3:45 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.