STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32N6570-DK unable to erase flash memory

I have just received my STM32N6570-DK and tried to flash the external memoryWhatever I do :* program an Hex file* erase single sector* erase full memory I always have the same error : failed to erase memoryI have tried to revert cube programmer to ve...

benabes by Associate
  • 1095 Views
  • 4 replies
  • 0 kudos

Resolved! Can't program STM32N6570-DK on macOS?

Hi, I am trying to bring up some software on an STM32N6570-DK.I'm able to upload example code from the STM32CubeIDE when the board is in DEV mode, e.g. when BOOT1 is set to 1. I followed the steps in this KB article: FSBL Explained However, I am unab...

jmole_0-1759444960595.png
jmole by Associate
  • 580 Views
  • 1 replies
  • 0 kudos

Resolved! FDCAN Bootloader in STM32G474RCT6

I am using STM32G474RCT6 microcontroller, I want perform firmware upgrade through CAN communication. But my controller doesn't provide the feature of Firmware upgrade through CAN communication.is there any possibility to use CAN communication for fir...

Sri_Nishanth_0-1701082492037.png

Resolved! flash a program on STM32N6570DK

  Hi, I created a project on the STM32N6570DK and I only have the project "in (STM32CubeIde)", I don't have the FSBL and the Appli. How do I flash my firmware? I tried to use the fsbl provided by the official ST repository, namely "ai_fsbl.hex", but ...

elena01 by Associate
  • 699 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.