STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

internal flash memory not programmed

Hi , i want to program a stm32f030f4p6 mcu with st-link but this problem is appeared for me : when i connect to the mcu i can erase chip easily , but when i program it , the content of flash memory not changed , the value of all blocks in flash memo...

0690X000009YDK3QAO.png

STM32CubeProgrammer not detecting ST-Link devices

I am running Windows 7 and v2.1.0 of the STM32CubeProgrammer. It is unable to find connected ST-Link devices (in this instance, an ST-Link/V2, a Nucleo STM32F411RE, and a Nucleo STM32F303RE).However, if I click the "Firmware Upgrade" button, it is a...

MZimm.13 by Associate
  • 1535 Views
  • 2 replies
  • 0 kudos

Uninstall STM32CubeProgrammer Ubuntu

I've been trying to install this crap for the past 3 hours now. I've had to purge OpenJDK completely from my PC and install Oracle Java and I still keep getting the same damn error: "You are using OpenJDK, please install Open JFX". I'm now trying to ...

BRho by Associate II
  • 6335 Views
  • 5 replies
  • 1 kudos

No DFU detected

Hi I'm running the STM32CubeProgrammer on MacOs and I'm trying to connect a cheap STM32F407ZG to upload a program via USB the the programmer cannot connect to the board. Anyone got any ideas?

GHalb by Associate II
  • 7321 Views
  • 5 replies
  • 0 kudos

Erase concept in flashing phase

Hello, when we flash binary file by using st link utility or cube programmer, previously flashed binary data are automatically erased ?For example, flashing to head of sector 0. If previously flashed code size is bigger than new one, previously code ...

KKane by Associate II
  • 1228 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.