STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Unable to communicate with the STM32H747i MCU

I have an STM32H747i-Eval board, I am unable to flash/access the MCU using any of the STM32 tools like,STlink utility I get the following error when i try to connect 18:07:28 : Can not connect to target!          ...

VishwasM by Associate
  • 1275 Views
  • 1 replies
  • 0 kudos

no javagfx.propertises file

I am using ubuntu18.04. I've installed open jdk amd javagfx. But cube prog does not run due to javagfx.properties file. I searched under /usr directories. But I couldnt find out it at all.Could anyone help me?

Clee.4 by Associate II
  • 664 Views
  • 0 replies
  • 0 kudos

STM32 Bootloader stuck in loop

Hello,I am trying to use the built-in UART bootloader on an STM32H7. I have two boards: one on which the bootloader works, and one on which it cannot connect.The board on which I cannot use the bootloader reports the following error when I try to con...

0690X00000AQmFVQA1.png
ST User by Associate III
  • 959 Views
  • 0 replies
  • 0 kudos

How to compile API with QT

Hello, I have tried to compile the API examples of the STM32CubeProg with Qt but as one of the DLLs is 64 bits, it fails to run. Is there any compiled version of the DLL for 32 bits?Regards,

luisf by Associate II
  • 1592 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.