2024-12-09 9:44 AM
I have installed STM32duino and using Arduino IDE to program STM32F407VG. I have set the upload method to 'STM32CubeProgrammer(DFU). Arduino IDE fails to program the Board. However when I download the .bin file created from Arduino IDE using the Cube Programmer, it works fine. Can somebody help me to set the system so that I can directly program the board using the Arduin IDE.
2024-12-09 10:09 AM
You should probably ask this in the STM32duino forum - that's the official place for STM32duino support:
2024-12-09 10:14 AM
>>I have set the upload method to 'STM32CubeProgrammer(DFU)..
Sounds like you haven't..
Perhaps you can use an ST-LINK/V2-1 or V3 that permits for a drag-n-drop of the .BIN into a USB MSC drive.
Problems with Arduino IDE, perhaps converse with Arduino, and their forum?
2025-03-28 8:14 AM - last edited on 2025-03-28 8:19 AM by Andrew Neil
Selecting 'STM32CubeProgrammer(DFU)' requires you boot your board in dfu mode.
to know how boot in the correct mode depending of your mcu.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.